The Event Manager Database allows the creation, viewing, and editing of all alarms and events in your project. Events, such as tag value changes, screen changes, and even the time of day, can trigger specific "actions". Actions can include changing tag values, copying tag values, playing a sound, changing the current screen, taking a screen capture, sending e-mail, or popping-up a message box. Here's more info about Alarms, Messages and Events.
The Panel Manager allows general setup for project functions like the screen saver, alarm list size and enable/disable of the beeper. The panel manager is also where you configure PLC communication settings. |
The Tag Name Database shows all the currently configured tags in your project, along with all the details about each tag. New tags can be added here as well as when an object is created. Tags can be assigned to PLC memory locations or can be internal to the C-more panel. There are also a number of internal system tags that can be used for various functions. Download the demo software to explore the tag name database and the internal and systems tags.
|