Home | Store | Product Selector | Feedback | C-more Micro
AutomationDirect logo
C-more logo
   Back to: Home  |  Software
   
Software links
Objects
Click to expandSetup & Database
Download the Demo
Sample Projects
Improvements in C-more
buy now
Purchase the full version for $129
Test Your Screens in the Simulator
Troubleshoot your project on the PC without a PLC or a panel.
C-more Software Objects
Objects
Below is a complete list of the objects available in the C-more programming software. Mouse over any object for a sample of that object.
HMI screens are created by "dragging" objects from the object list and "dropping" them into the workspace.
• Objects can be sized to a grid, or freeform. Objects can be ordered and grouped. See the toolbar section for more about object manipulation.
• Objects are even allowed to overlap. For example, you can put a bitmap graphic on top of a screen change pushbutton. The bitmap will display, and the underlying button will function when pressed. If two touchable object are overlapped, only the object on top will function when touched

 
 
AutomationDirect.Com © 2005 | Privacy Policy