Home | Store | Product Selector | Feedback | C-more Micro
C-more logo
   Back to: Home  |  Hardware  |  Accessories
   
Hardware links
Improvements in C-more
Ready to Purchase C-more?
Visit our online store or call us to place an order: 1-800-633-0405.
If you have any questions about C-more
please contact us via email or phone.

Expansion Assembly
This expansion assembly mounts on to the back of a C-more panel and will accept two expansion modules. Additional expansion modules will be available in the future, but the CF Card Interface Module is the only expansion module at this time. The CF Card Interface Module can only be used in the right-hand slot.
 
 
AutomationDirect.Com © 2005-2012 | Privacy Policy