Home | Store | Product Selector | Feedback | C-more Micro
C-more logo
   Back to: Home  |  Features  |  Communication Features
   
Feature links
Improvements in C-more
Yes,
We Have an App for That!


The C-more Remote Access feature now supports the iOS with the C-more Remote HMI'App' for your iPad, iPhone(3G or later), or iPod touch.
C-more Remote Access & Control
NEW! Access your C-more Panel from your iPad®, iPhone®, or iPod touch®²
The C-more Remote Access feature now supports the iOS with the C-more Remote HMI  'App' for your iPad, iPhone(3G or later), or iPod touch. Simply configure the network settings in the panel project and connect the panel to a network. (This feature requires firmware version 2.73 or later to function.¹)
c-more iphone app
C-more app for iPad
Control Engineering choice award
Control your machine or process from your mobile device as though you are physically in front of the C-more Panel (with 'Full Control mode'), or configure the settings for 'View Only', or 'View and Screen Change Only' for more presence sensitive projects. And remember, C-more supports password security at the object level, so you can limit access to certain controls even if the 'Full Control' access option is selected.
C-more Remote Access is also available on your PC, with our free browser based version.
Download Now - Just $4.99
Download the C-more Remote App from the App StoreSM² here
Available on the Apple Store
Authorized users have the ability to remotely:
• Monitor and control screen operations of the C-more panel as if touching the panel itself
• Test and troubleshoot the C-more project
• The iPhone or apple Zoom feature allows the user to zoom in on specific objects or areas of the screen for viewing clarity
• Users can save jpeg screen captures (at any zoom level) to review, email and print if needed
Multilevel Logon Security³
Three Remote Access user accounts can be configured and stored in the panel project. Each account allows up to five remote users to be connected simultaneously.
Multilevel Access Control
Each account can be configured in one of the following levels of access:
• View Only
• View and allow Screen Change only
• Full Control
Lockout/Tagout Functionality
Activation or Notification Tags provide an option for each account to have associated user configurable TAGS that allow the Panel project or PLC project to indicate that a remote user is connected, or to enable or disable the remote access feature. These tags can be used to activate alarms, events or notifications to alert local operators that a remote user is connected. The Disable/Enable TAGS can be assigned to a switch to allow local operators the ability to enable or disable the remote access feature for security or safety reasons.
¹ Firmware updates are downloadable for authorized customers here.
² Apple, iPad, iPhone, and iPod touch are trademarks of Apple Inc., registered in the U.S. and other countries. App Store is a service mark of Apple Inc.
³ While C-more Remote Access is password protected, AutomationDirect strongly encourages the use of additional security measures (including - but not limited to - firewalls & VPNs) where appropriate and applicable.
 
 
AutomationDirect.Com © 2005-2012 | Privacy Policy