Home | Store | Product Selector | Feedback | C-more Micro
AutomationDirect logo
C-more logo
   Back to: Home  |  Features  |  Optional Features
   
Feature links
Improvements in C-more
C-more Protects
Your Investment

and offers hundreds of improvements over our previous touch panels.
C-more Expansion Assembly
This expansion assembly mounts on to the back of a C-more panel and will accept two expansion modules. Additional expansion modules will be available in the future, but the CF Card Interface Module is the only expansion module at this time. The CF Card Interface Module can only be used in the right-hand slot.
 
 
AutomationDirect.Com © 2005 | Privacy Policy